Model libraries for PSpice®

PSpice is a high performance SPICE simulator that is used in combination with OrCAD Capture to simplify the design and testing of both analog and mixed signal circuits. The software is sold and maintained by Cadence Design Systems. Included in PSpice is a limited library of Coilcraft RF inductor models.

Coilcraft has created a set of advanced frequency dependent models for modelling the small signal response of inductors. These models are based on the same schematic, element values, and coefficients for variable elements which are provided in our SPICE model documents for each inductor series. 

Download Coilcraft Advanced model libraries 

To include the advanced library copy the contents of the Coilcraft_PSpiceLib.zip file to a location that makes sense. For example create a new libraries folder in the PSpice install directory C:\Cadence\Libraries Alternatively if installing for a single user the path can point to a folder in the user’s documents folder. See below for more detailed instructions

Coilcraft_PSpiceLib.zip Includes all Coilcraft power and RF inductors for AC analysis.

Installing Coilcraft Advanced model libraries 

  1. Download the Coilcraft_PSpiceLib.zip file
  2. Extract the .zip file and navigate into the extracted folder
    Picture1.png
  3. Copy the contents from the extracted folder
  4. Navigate to “C:\Cadence"
    • This should be the default  install location for OrCAD/PSpice 
    • Create a new folder and name it Libraries

    *Alternatively these files can be placed anywhere that makes sense to the user
  5. Paste the files from the Coilcraft_PSpiceLib.zip here
    • If you already have the Coilcraft Advanced model library and are updating you will need to choose to replace the destination files.

    Picture2.png

Using Coilcraft Advanced models

  1. To use a Coilcraft Advanced inductor model simply select the place part icon
    Picture3.png
  2. Click on Add Library and once you have navigated to the location you saved the library files to select Coilcraft_PSpiceLib.olb
    Picture4.png
  3. Ensure the library is included in the simulation settings
    • Settings can be accessed when creating a new simulation profile or by editing the current one
    • Select the configuration files tab and with the library category highlighted browse to the save location selecting Coilcraft_PSpiceLib.lib
    • Select Add as Global to make the library available for future use or Add to Design to add the library for only the current design.

    Picture5.png
  4. With the Coilcraft_PSpiceLib library selected search the parts list for the inductor you want to include in your design. Double clicking the part number will select it and allow the placing of the inductor onto the schematic.
    Picture6.png

Plotting Waveforms 

To plot Inductance vs frequency:
IMG(V(Vin)/I(R2))/(2*pi*frequency)
To plot Impedance vs frequency:
V(Vin)/I(R2)
To plot ESR vs frequency:
R(V(Vin)/I(R2))
To plot Q factor vs frequency:
ABS(IMG(V(Vin)/I(R2))/R(V(Vin)/I(R2)))
*note voltage node names may be different it is up to user to ensure voltage is across inductor